Configure references
The topics in this section contain detailed reference information that pertains to configuring Power Operation.
Use the links in the following table to find the content you are looking for:
| Topic | Content |
|---|---|
| Citect INI Parameters | A detailed listing of the Citect INI parameters you can use in your projects. |
| Logic code definitions | Design considerations and sample architectures for the Power Operation components. |
| Default Genie Library | A detailed listing of the Power Operation PLS_* genie library and its naming conventions. |
| Deadbands and ignored devices and topics | Deadbands and ignored devices and topics let you limit information that you see in system queries and data acquisition from applications that use the Schneider Electric CoreServiceHost. |
| Add engineering unit templates, units, and conversions | Detailed information on how to set up and add engineering units and conversions. |
| LiveView Tables | Detailed information on the information contained in each LiveView table. |
| Notifications references | Detailed information on the notifications user interfaces (UIs). |
| Web Applications references | Detailed information on configuration the Web Applications. |